Flash programming

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Flash programming

6,076 次查看
marchè
Contributor I
Hi..
When the micro is in the secure state, Can I program the flash memory from within the bootloader?
Or the bootloader must leave the micro in unsecured state?
 
Thanks...
 
 
标签 (1)
0 项奖励
回复
3 回复数

2,081 次查看
Ilocano
Contributor I
With the 9S12C32 in secure mode it is possible to erase and program FLASH. I added things to the SErial mon for this purpose.
0 项奖励
回复

2,081 次查看
imajeff
Contributor III
AFAIK, If there are no errata stopping it, then the bootloader can have full rain on the Flash within secure mode. In fact, if it were not able to erase Flash, then the MCU could not be unsecured so it is in the design.
0 项奖励
回复

2,081 次查看
Lundin
Senior Contributor IV
There is an errata stopping it for the old "B" masks:

In normal single chip mode, when security is enabled, it is not possible to launch the Program ($20), Sector-Erase ($40) and Erase- Verify ($05) commands in the Flash. The Mass-Erase ($41) command can be launched.

Same goes for EEPROM.
0 项奖励
回复