Flash Memory updation

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Flash Memory updation

Jump to solution
1,777 Views
rahulkrishna
Contributor IV

Hi,

I have some calibration constants and i allocated some fixed locations of Flash memory for these calibration constants. My doubt is because of some reasons i want to change these calibration constants during run time, how to change the value while running the code without actually flashing through debugger. i will be sending the new value through the CAN using some message id and the data contains the new calibration constant, I need to read this updated calibration constant and update the flash memory. Is it possible?  i am using the s12xEQ variant.

 

Thanks.

Labels (1)
Tags (2)
0 Kudos
Reply
1 Solution
1,636 Views
rahulkrishna
Contributor IV

I think D flash is the way to go.

View solution in original post

0 Kudos
Reply
1 Reply
1,636 Views
rahulkrishna
Contributor IV

I think D flash is the way to go.

0 Kudos
Reply