First Projects using Freescale S12

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

First Projects using Freescale S12

1,092件の閲覧回数
rayhall
Contributor V

I have just finished my first projects using the Freescale S12 MCU. I would like to thank everyone that help me.

 

In the past I have being using the Atmel AVR. The change to the Freescale was made easier with your help.

 

If there is one area were the AVR is a lot easier to work with, this is EEPROM. To me someone tried very hard to make it difficulty in the Freescale. Other then that I am very happy with the Freescale.

 

Here are pictures of the two projects.

 

 

http://www.turbofast.com.au/tfbin/CAN_EGT-8_PCB.jpg   Eight channel EGT Amplifer using the S12G128

 

http://www.turbofast.com.au/tfbin/CAN_InterfacePCB.jpg   CAN bus interface using the S12XE

 

Ray.

ラベル(1)
0 件の賞賛
返信
0 返答(返信)