First Projects using Freescale S12

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

First Projects using Freescale S12

1,088 次查看
rayhall
Contributor V

I have just finished my first projects using the Freescale S12 MCU. I would like to thank everyone that help me.

 

In the past I have being using the Atmel AVR. The change to the Freescale was made easier with your help.

 

If there is one area were the AVR is a lot easier to work with, this is EEPROM. To me someone tried very hard to make it difficulty in the Freescale. Other then that I am very happy with the Freescale.

 

Here are pictures of the two projects.

 

 

http://www.turbofast.com.au/tfbin/CAN_EGT-8_PCB.jpg   Eight channel EGT Amplifer using the S12G128

 

http://www.turbofast.com.au/tfbin/CAN_InterfacePCB.jpg   CAN bus interface using the S12XE

 

Ray.

标签 (1)
0 项奖励
回复
0 回复数