Exception handling for S12Z

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Exception handling for S12Z

2,735件の閲覧回数
jeffcharles
Contributor III

Hi,

After reset deassert, CPU starts running. The software will enable the watchdog(COP) during initialization. If the software crashes between startup and enabling the watchdog,
how can the CPU recover automatically without powering on again or pulling down the reset pin?

Best Regards,

Jeff

0 件の賞賛
返信
3 返答(返信)

2,725件の閲覧回数
lama
NXP TechSupport
NXP TechSupport

Hi,

 

You can enable the COP by HW and COP is enabled immediately after reset. It is done by writing bit NV[2..0] in the FOPT storage place in the flash memory at address 0xFF_FE0E. This value is then copied into the CPMUCOP register during reset sequence so COP is enabled automatically and immediately. Of course, in this case, writing CPMUCOP in the SW has no meaning because the CPMUCOP is write once only in the normal mode. The data sheet states:

Write:

  1. RSBCK: Anytime in Special Mode; write to “1” but not to “0” in Normal Mode
  2. WCOP, CR2, CR1, CR0:

— Anytime in Special Mode, when WRTMASK is 0, otherwise it has no effect

— Write once in Normal Mode, when WRTMASK is 0, otherwise it has no effect.

– Writing CR[2:0] to “000” has no effect, but counts for the “write once” condition.

– Writing WCOP to “0” has no effect, but counts for the “write once” condition.

 

This can be done by means of following code in the main.c file

// set COP second largest period NV[2..0] = 0001 => COPCTL_CR[2..0] will be 111 after reset

// set no COP window WCOP = 0 => NV3 must be NV3 = 1

// Chapter 1.13.2 COP Configuration

const unsigned char COP_HW_START   @ 0xFFFE0E= 0B00001000;

void main(void) {

 

Then in the S record you can find line:

S205FFFE0E08E7

 

The CodeWarrior uses macro     __RESET_WATCHDOG();   /* feeds the dog */

Which is defined as

  #define __RESET_WATCHDOG() (CPMUARMCOP = 0x55U, CPMUARMCOP = 0xAAU)

However, it can happen you want or must refresh the watchdog somewhere else where MCU’s registers are not included. In this case you have to either include registers header file or insert the code in the assembler form at appropriate place to ensure the COP does not overflow.

    asm {     MOV.B  #0x55,0x06CF;

                  MOV.B  #0xAA,0x06CF;

        }

 

Finally, if I use this approach (immediate COP enable) I would use it in a final step of design to avoid problems during debugging.

 

Best regards,

Ladislav

2,723件の閲覧回数
jeffcharles
Contributor III

Hi Ladislav,

Thank you. I'll try it later.

I also see that this chip has some exception interrupts, such as SPARE, TRAP, SWI, SYS and ME interrupts. Can you share relevant information?

Best regards,

Jeff

0 件の賞賛
返信

2,718件の閲覧回数
lama
NXP TechSupport
NXP TechSupport

Hi,

Have you already read the CPU reference manual Chapter 7?

https://www.nxp.com/webapp/Download?colCode=S12ZCPURM

Best regards,

Ladislav

0 件の賞賛
返信