Error while downloading the code to XET256 mounted on daughter card

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Error while downloading the code to XET256 mounted on daughter card

1,970 Views
s12x_Ashok
Contributor I
I have an XEP100 eval board on which i have mounted the daughter card (LFSMPB12XEIM). I have connected the debugger to the BDM connector on the daughter card. However, I am using the crystal that is mounted on the XEP100 eval board which is 4 Mhz.

Now, when i create a sample project using Code warrior 4.7 for the target XET256, and try to download the code (there is nothing really in the sample project, it is just the empty main function that appears default when you create the project) the error message "Error while writing to FFF8....101F8" appears on the screen. When i proceed further it says "Failed to load the P&E_Multilink_Cyclonepro.abs" file.

I have attached the command window details, if it sounds helpful.

I am looking forward to any help.

Regards,
Ashok
Labels (1)
0 Kudos
Reply
1 Reply

973 Views
CrasyCat
Specialist III
Hello
 
Did you look at this thread?
 
The message you are getting indicates you are trying to download code at address 10100-101F8, which is not correct.
 
CarsyCat
 
0 Kudos
Reply