EEPROM page failure -- fault

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

EEPROM page failure -- fault

1,437 Views
dino12
Contributor I

Hi,

 

 

I am using EEPROM S12X controller for an industrial automation side. Where we need to maintain multiple copy of some configuration data. Multiple copies are used because to maintain back-up of data.

 

 

 

My question is that if S12X -- can have 4k of eeprom, i.e 4 pages of size 1K.

 

 

Then in this case if one page of eeprom gets corrupted may be because of some reason. Then data in other 3 pages will also get corrupted ?

 

 

Or each page is an independent EEPROM corruption of one does not affect the other ?

 

 

Please suggest.

 

 

Regards,

 

 

Dino

 

Labels (1)
0 Kudos
Reply
1 Reply

1,269 Views
thakkarhimanshu
Contributor I

Hi,

In my opinion the EEPROM can be linearly addressed with global addressing as well. As such there are not four different EEPROMs. Paging is done so that the entire memory addressing can fit into 64K of addressing. If for some reason the data on one page gets corrupted ( or in other words if some part of EEPROM is corrupted), then there are strong chances that the entire EEPROM is corrupted i.e. data on all the pages is corrupted. In any case the corruption of data on one page certainly means that data is not reliable.

Regards,

Himanshu