IIC on MC9S12DT256 with APS12DT256SLK

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

IIC on MC9S12DT256 with APS12DT256SLK

ソリューションへジャンプ
1,145件の閲覧回数
johndoe___
Contributor I

Hey!

 

I recently purchased a product, a LiPo Fuel Gage from SparkFun, without realizing that it was an IIC device! I've been trying to learn how to send the data to an LCD screen on my HCS12 device, but I'm struggling. I've been using the S12IICV2, AN3291, and AN2318 documents in an attempt to learn how this works, but I'm not sure I'm completely understanding it. I do have some sample code, but I don't really think it's helping me much honestly. It would be awesome if I could get some support.

 

Thanks.

ラベル(1)
0 件の賞賛
返信
1 解決策
984件の閲覧回数
RadekS
NXP Employee
NXP Employee

There is simple example code for S12NE64 (use the same IIC module) and communication with external EEPROM. You can take it as inspiration.

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
985件の閲覧回数
RadekS
NXP Employee
NXP Employee

There is simple example code for S12NE64 (use the same IIC module) and communication with external EEPROM. You can take it as inspiration.

0 件の賞賛
返信