Does S9ZVL12MLF chip have can interface?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Does S9ZVL12MLF chip have can interface?

ソリューションへジャンプ
4,318件の閲覧回数
nujia
Contributor I

I am using the DEVKIT-S12ZVL.      I downloaded the example from NXP.com .  The example is ZVL32MLF, and works ok.     The part ID is 0x04150000.     But the picture is S9ZVL12MLF.   

nujia_0-1640734053084.png

nujia_1-1640734378318.png

So  is S9ZVL12MLF  ZVL32MLF or ZVLA12MLF?   

The difference between the two chips is that one consists of CAN and the other does not have CAN.

Thanks.

 

0 件の賞賛
返信
1 解決策
4,259件の閲覧回数
danielmartynek
NXP TechSupport
NXP TechSupport

Hello @nujia,

Thank you for the information.

I see, either the ID register or the label is incorrect.

I can't explained it, I'm sorry for all the inconvenience.

You can read SRAM at 0x1400 which is unimplemented on S12ZVL32.

If Machine exception rises, the part is S12ZVL32

danielmartynek_0-1641136832094.png

 

Regarding the download link, thank you for pointing it out, let me report it.

 

Regards,

Daniel

 

元の投稿で解決策を見る

0 件の賞賛
返信
4 返答(返信)
4,297件の閲覧回数
nujia
Contributor I

Thank you, Daniel martynek,

nujia_0-1640830105272.png

nujia_1-1640830168639.png

 

I think the S9ZVL12MLF is ZVL32MLF.    So I plan to buy s9zvl128mlf development board.

But there is a wrong code download link.

nujia_2-1640830814883.png

 

0 件の賞賛
返信
4,260件の閲覧回数
danielmartynek
NXP TechSupport
NXP TechSupport

Hello @nujia,

Thank you for the information.

I see, either the ID register or the label is incorrect.

I can't explained it, I'm sorry for all the inconvenience.

You can read SRAM at 0x1400 which is unimplemented on S12ZVL32.

If Machine exception rises, the part is S12ZVL32

danielmartynek_0-1641136832094.png

 

Regarding the download link, thank you for pointing it out, let me report it.

 

Regards,

Daniel

 

0 件の賞賛
返信
4,206件の閲覧回数
nujia
Contributor I

Hi , Daniel,

         Thank you,   It runs to the Machine exception ISR.  So it is S12ZVL32.  

nujia_0-1642555425401.png

 

0 件の賞賛
返信
4,305件の閲覧回数
danielmartynek
NXP TechSupport
NXP TechSupport

Hello @nujia,

Can you show a screenshot of the ID register in the memory view?

 

Thanks,

BR, Daniel

 

0 件の賞賛
返信