Development Board - S12XE

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Development Board - S12XE

3,786件の閲覧回数
ptmy
Contributor I

Hi,

 

I am looking for development kit for S12XE family micro controller. Please suggest? Any electronics dealers available in Chennai.

 

-Thiru

ラベル(1)
6 返答(返信)

3,335件の閲覧回数
mac164
Contributor II


I recently purchased a XEP100 from TechnologicalArts that works good.

The XGATE assembler has problems and I was able to finally develope a XGATE Serial transceiver.  I recall serveral request in the past for an example of an XGATE Serial program. I excerted a part of my program to assist some friends and they though it would be helpfull for the forum...

The enclosed file (XG_TUT_02) may assist you in developement...

3,335件の閲覧回数
Monica
Senior Contributor III

WOW Leonard, thanks for sharing! :smileygrin:

0 件の賞賛
返信

3,335件の閲覧回数
Monica
Senior Contributor III

Hello, Thirumoorthy

How is the project going? Was this helpful?

Please let us know! :smileywink:

Best regards,

Monica

0 件の賞賛
返信

3,335件の閲覧回数
ptmy
Contributor I

Hi Monica,

I need to purchase the development kit, but i didn't receive the details.

Please provide the kit and price details to proceed further.

Regards,

Thirumoorthy P

On Tue, Apr 16, 2013 at 2:42 AM, Monica Arvizu <

0 件の賞賛
返信

3,335件の閲覧回数
iggi
NXP Employee
NXP Employee

These are the part numbers of two development boards:

- DEMO9S12XEP100  

- EVB9S12XEP100

Use the link below to see the prices:

DEMO9S12XEP100 Product Summary Page

EVB9S12XEP100 Product Summary Page

Use Distributor (blue) button and select country to see availability of the boards.

Also , you may contact distributor directly in India. Use this link:

Distributor Network

Regards,
Ivan

3,335件の閲覧回数
RadekS
NXP Employee
NXP Employee

I would like to recommend for example DEMO9S12XEP100 board:

www.freescale.com/webapp/sps/site/prod_summary.jsp?code=DEMO9S12XEP100

or EVB9S12XEP100 board:

http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=EVB9S12XEP100

Important note:

Unfortunately both boards contains onboard BDM interface from SofTec and their interface drivers is not supported under 64bit OS.

Authors of this interfaces terminated cooperation with Freescale and henceforth they did not support these products.

There are possible solutions:

  1. Different BDM Interface. For example P&E USB Multilink Interface:

          http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=USBMULTILINKBDM

  1. Different operational system. For example any 32bit windows.
  2. Intall virtual PC, Windows XP Mode 32bit, Install CW and drivers...

http://en.wikipedia.org/wiki/Windows_Virtual_PC

Freescale Authorized Distributors

http://www.freescale.com/webapp/sps/site/overview.jsp?code=DISTRIBUTORS