Derivative could not be unsecured

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Derivative could not be unsecured

2,519 Views
liuweiwei
Contributor I

mc9s12xdp512.  I want to unsecure the mcu, but it failed everytime. But other mcu can be unsecured. Can you tell me is there some way to unsecure or is it broken?

0 Kudos
Reply
2 Replies

2,256 Views
RadekS
NXP Employee
NXP Employee

Hi Liu,

Additionally please check whether MCU is correctly powered and gated (XCLKS pin,…).

Please check also BDM cable orientation…

Please touch MCU by finger. When MCU is hot, it is probably damaged...

I hope it helps you.

Have a great day,
Radek

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

2,256 Views
danielmartynek
NXP TechSupport
NXP TechSupport

Hi,

You can unsecure the MCU in CW debugger mode

HCS12MultilinkCyclonePro -> Unsecure

If this doesn’t work, you can use PEmicro Unsecure12 utility.

 

Regards,

Daniel

0 Kudos
Reply