Derivative could not be unsecured

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Derivative could not be unsecured

2,502件の閲覧回数
liuweiwei
Contributor I

mc9s12xdp512.  I want to unsecure the mcu, but it failed everytime. But other mcu can be unsecured. Can you tell me is there some way to unsecure or is it broken?

0 件の賞賛
返信
2 返答(返信)

2,239件の閲覧回数
RadekS
NXP Employee
NXP Employee

Hi Liu,

Additionally please check whether MCU is correctly powered and gated (XCLKS pin,…).

Please check also BDM cable orientation…

Please touch MCU by finger. When MCU is hot, it is probably damaged...

I hope it helps you.

Have a great day,
Radek

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

2,239件の閲覧回数
danielmartynek
NXP TechSupport
NXP TechSupport

Hi,

You can unsecure the MCU in CW debugger mode

HCS12MultilinkCyclonePro -> Unsecure

If this doesn’t work, you can use PEmicro Unsecure12 utility.

 

Regards,

Daniel

0 件の賞賛
返信