Default level of GPIO

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Default level of GPIO

1,275 Views
528887301
Contributor II

What is the default level of GPIO after S12XET256  power up and befor control?

1 Reply

1,153 Views
dianabatrlova
NXP TechSupport
NXP TechSupport

Hi,

In the RM you can see specification for each available port. Some of them has GPIO function after reset. In the DDRx register for associated port you can see default state for associated pin. For example, Port P is configured as input (see DDRP) and in the PERP register you can see default state of pull device. Pull device is disabled.

I hope it helps you.

Best regards,

Diana