Default level of GPIO

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Default level of GPIO

1,293件の閲覧回数
528887301
Contributor II

What is the default level of GPIO after S12XET256  power up and befor control?

タグ(1)
1 返信

1,171件の閲覧回数
dianabatrlova
NXP TechSupport
NXP TechSupport

Hi,

In the RM you can see specification for each available port. Some of them has GPIO function after reset. In the DDRx register for associated port you can see default state for associated pin. For example, Port P is configured as input (see DDRP) and in the PERP register you can see default state of pull device. Pull device is disabled.

I hope it helps you.

Best regards,

Diana