Debugger connection error

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Debugger connection error

1,788 Views
pratibhasurabhi
Contributor V

Hi,

I am currently using codewarrior 10.7 on windows 10 - 64bit os. 

I am not able to download the code using debugger on board S12ZVML128 MCU, i am attaching the snap of the error message which is popping everytime whenever i click debug button on codewarrior 10.7 

pratibhasurabhi_0-1608118135006.png

 

pratibhasurabhi_1-1608118178863.png

I also Re-installed the CodeWarrior and tried to debug another workspace but still it is showing the same error message.

Suggest me method in order to fix this issue.

Thanks!

0 Kudos
Reply
1 Reply

1,766 Views
dianabatrlova
NXP TechSupport
NXP TechSupport

Hello,

 

Have you checked the user guide of the board, power supply, jumper settings?

https://www.nxp.com/webapp/Download?colCode=MC9S12ZVM128MCBUG

When you check the connection in the debug configuration, have you seen the port?

For example:

dianabatrlova_0-1608293171520.png

Thank you,

Best regards,

Diana

0 Kudos
Reply