DSP56F800 - USB interface JTAG programmers

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

DSP56F800 - USB interface JTAG programmers

4,153 Views
Devendra
Contributor I
We are currently using Parallel port (25-pin) to JTAG (10-pin) interface for programming DSP56F800 and MC56F8300 series controllers.
 
I would like to know if there is any USB interfaced JTAG programmer, because modern day Laptops don't have a parallel port.
 
Any converter for USB to Parallel port should work for this? There are some converters available which emulate a parallel port through a coverter hardware and some device driver installed in the PC.
 
Please reply ASAP.
 
Thanks and Best Regards,
Devendra

--
Alban Edit: Please always include FSL Part Number in Message Subject line.
http://forums.freescale.com/freescale/board/message?board.id=FORUMUSE&message.id=865



Message Edited by Alban on 2007-10-15 02:23 PM
Labels (1)
0 Kudos
Reply
2 Replies

1,852 Views
Cowboy
Contributor I
0 Kudos
Reply

1,852 Views
Cowboy
Contributor I
Hi Devendra
 
Here are some sites that you can order from.
 
 
I havend tested one of these, but I'm pretty sure they will work
 
 
0 Kudos
Reply