I just bought an NE64 dev board and am currently in the process of trying to get to accept a dhcp address. I hacked apart the connecterapp and NE64_Vend_OpenTcp to try to make my own project. Please let me know what i am doing wrong here. Here is what i got so far:
/**************************************************************************
*
* Copyright (C) 2003 Freescale Semiconductor, Inc.
* and 2000-2002 Viola Systems Ltd.
* All Rights Reserved
*
* File Name : Main.c
* Project Name : Connector_App.mcp
* Description : This file contains main() for the Connector_App demo
* code for the MC9S12NE64.
* It does initializations and calls functions in the
* Connector_App.c application code. The Connector_App.c
* file contains code for IO communication and UDP
* protocol functions on the MC9S12NE64.
*
* *** NOTE: This project is for demonstration purposes only. It excludes
* portions of the complete OpenTCP Stack for other protocols,
* such as http, bootp, dns, etc. The complete version of this
* stack is also included in the MC9S12NE64 Resource CD.
*
* *** NOTE: All header files have been removed from the Connector_App.mcp
* project due to the 32-file limit of CodeWarrior Special
* Edition. However, all the header files are included in your
* working folder and can be viewed by highlighting it's name
* in a source file, right clicking, and choosing "Find and
* Open File..." You may also just type the name of the file
* in any source file and do this.
*
* Version : 1.1
* Date : 07/21/04
*
***************************************************************************/
#include "Connector_App.h"
#include "ne64api.h"
#include "ne64config.h"
#include "ne64debug.h"
#include "ne64driver.h"
#include "mBuf.h"
#include "debug.h"
#include "datatypes.h"
#include "timers.h"
#include "system.h"
#include "ethernet.h"
#include "arp.h"
#include "dhcpc.h"
#include "icmp.h"
#include "ip.h"
#include "udp.h"
#include "tcp_ip.h"
#include "address.h"
#include "MC9S12NE64.h"
/* Including used modules for compiling procedure */
/* Network Interface definition. Must be somewhere so why not here? :-)*/
struct netif localmachine;
extern void RTI_Init (void);
extern void RTI_Enable (void);
//extern void porth_isr_handler (void);
extern tU08 gotlink;
extern UINT8 dhcpc_state;
void Wait_for_UpdTcp(void);
#if USE_SWLED
tU16 LEDcounter=0;
#endif
//============================================================
tU08 OldSwitchValue=255;
tU16 Pot=0;
tU16 OldPot=1050;
tU08 OldB1=255;
tU08 OldB2=255;
//============================================================
//Initialize ATD
//============================================================
void ATD_init(void)
{
ATDCTL2 = ATDCTL2_ADPU_MASK | ATDCTL2_AFFC_MASK;
ATDCTL3_S1C = 8; // 8 ch seq.
ATDCTL3_FIFO = 0; // no FIFO
ATDCTL3_FRZ = 3; // Freeze immediately in BDM
ATDCTL4 = ATDCTL4_PRS2_MASK |ATDCTL4_PRS1_MASK | ATDCTL4_PRS0_MASK;
ATDCTL4 = ATDCTL4 & ~ATDCTL4_SRES8_MASK; //10 bit
ATDCTL5 = ATDCTL5_SCAN_MASK;
}
//============================================================
// Initialize Port for LEDs, Switch, and Buttons
//============================================================
void demoinit(void)
{
//LEDS
DDRG_DDRG0 = 1;
DDRG_DDRG1 = 1;
PTG_PTG0 = 1; //turn off
PTG_PTG1 = 1; //turn off
//SWITCH (RUN/LOAD) 0:input
DDRG_DDRG4 = 0;
//BUTTON2
DDRH_DDRH4 = 0;
PIEH_PIEH4 = 1; //PIEH4 Interrupt Enable
}
//============================================================
/* main */
//============================================================
void main(void)
{
//INT16 len;
long timeout;
char Got_dhcp=TRUE;
/* System clock initialization */
CLKSEL=0;
CLKSEL_PLLSEL = 0; /* Select clock source from XTAL */
PLLCTL_PLLON = 0; /* Disable the PLL */
SYNR = 0; /* Set the multiplier register */
REFDV = 0; /* Set the divider register */
PLLCTL = 192;
PLLCTL_PLLON = 1; /* Enable the PLL */
while(!CRGFLG_LOCK); /* Wait */
CLKSEL_PLLSEL = 1; /* Select clock source from PLL */
INTCR_IRQEN = 0; /* Disable the IRQ interrupt. IRQ interrupt is enabled after CPU reset by default. */
/* initialize processor-dependant stuff (I/O ports, timers...).
* Most important things to do in this function as far as the TCP/IP
* stack concerns:
* - initializing some timer so it executes decrement_timers
* on every 10ms (TODO: Throw out this dependency from several files
* so that frequency can be adjusted more freely!!!)
* - not mess too much with ports allocated for Ethernet controller
*/
_INIT_DEBUG();
ATD_init();
demoinit();
RTI_Init();
/* Ethernet (MAC) address */
localmachine.localHW[0] = hard_addr[0];
localmachine.localHW[1] = hard_addr[1];
localmachine.localHW[2] = hard_addr[2];
localmachine.localHW[3] = hard_addr[3];
localmachine.localHW[4] = hard_addr[4];
localmachine.localHW[5] = hard_addr[5];
/* Init system services */
timer_pool_init();
/* Initialize all buffer descriptors */
mBufInit ();
/* Initialize all network layers */
EtherInit();
//Enable RTI
RTI_Enable ();
//Initialize required network protocols
(void)arp_init();
(void)udp_init();
(void)tcp_init();
while (!gotlink){
}
/* if using DHCP, following network variables should be initialized to zero
* during startup (or to previously-assigned parameters if they are stored
* somewhere - in FLASH maybe...)
*/
/* Note: If enabled, this function initializes the DHCP protocol */
localmachine.localip = 0;
localmachine.defgw = 0;
localmachine.netmask = 0;
(void)dhcpc_init();
timeout = 1600000; // This timeout is Application,and frequency dependent
while (dhcpc_state != DHCP_STATE_BOUND){
dhcpc_run();
Wait_for_UpdTcp(); //wait for it
timeout--;
if (timeout == 0)
{
Got_dhcp = FALSE;
break;
}
}
if(Got_dhcp==FALSE){
/* Set our network information. This is for static configuration.*
* if using BOOTP or DHCP this will be a bit different. */
/* IP address */
localmachine.localip = *((UINT32 *)ip_address);
/* Default gateway */
localmachine.defgw = *((UINT32 *)ip_gateway);
/* Subnet mask */
localmachine.netmask = *((UINT32 *)ip_netmask);
}
/* main loop */
DEBUGOUT(">>>>>>>>>Entering to MAIN LOOP>>>>>>>>>\n\r");
for (;
{
#if USE_SWLED
UseSWLedRun();
#endif
if (gotlink) {
/* Try to receive Ethernet Frame */
Wait_for_UpdTcp();
/* Application main loops */
/* manage arp cache tables */
arp_manage();
if(Got_dhcp==TRUE){
dhcpc_run ();
PTG_PTG1 = 0; //turn on LED2
}
else{
PTG_PTG0 = 0; //turn on LED1
}
}
/* Application main loops */
/* TCP/IP stack Periodic tasks here... */
//udp_demo_run();
}
}
//---------------end of main----------------------------------------
//---------------start of function declarations
void Wait_for_UpdTcp(void){
INT16 Pack_len;
if( NETWORK_CHECK_IF_RECEIVED() == TRUE )
{
switch( received_frame.protocol)
{
case PROTOCOL_ARP:
process_arp (&received_frame);
break;
case PROTOCOL_IP:
Pack_len = process_ip_in(&received_frame);
if(Pack_len < 0)
break;
switch (received_ip_packet.protocol)
{
case IP_ICMP:
process_icmp_in (&received_ip_packet, Pack_len);
break;
case IP_UDP:
process_udp_in (&received_ip_packet,Pack_len);
break;
case IP_TCP:
process_tcp_in (&received_ip_packet, Pack_len);
break;
default:
break;
}
break;
default:
break;
}
/* discard received frame */
NETWORK_RECEIVE_END();
}
}