DEMOAX9S12XEP100 drivers

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

DEMOAX9S12XEP100 drivers

2,109 Views
jackjamieson
NXP Employee
NXP Employee

I am looking for the driver that allows me to communicate with the demo board.

 

When I first installed CW, an “in circuit debugger” driver that allowed me to communicate with the board came up but it did not install correctly.  When I went to re-install the driver CW could not find the driver online. 

 

Any thoughts?  I need this to program the board through the USB cable provided in the kit.   

Labels (1)
Tags (2)
3 Replies

1,896 Views
iggi
NXP Employee
NXP Employee

Quite strange. I just connected a brand new board to the PC and the drivers were installed correctly (ready to use).

What OS do you use? I'm not usre if there a problem with 64-bit Windows OS version.

Check the Device and Printers and see if you have device as in picture below:
Capture2.JPG

If not you can try and re-install the PEmicro drivers:

https://www.pemicro.com/downloads/download_file.cfm?download_id=301

In CW project, a connection to be used with this setup is P&E USB Multilink BDM.

Regards,

iggi

1,896 Views
jackjamieson
NXP Employee
NXP Employee

Thanks, Iggi! My customer had to use a BDM connector with a programming tool and is good to go now!

1,896 Views
iggi
NXP Employee
NXP Employee

Good. We actually use the BDM programmer rather than OSBDM.

0 Kudos
Reply