DEMO9S12XDT512 CAN DRIVER

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

DEMO9S12XDT512 CAN DRIVER

2,076件の閲覧回数
candriver
Contributor I

DEAR FRNDS i m using DEMO9S12XDT512 EVB....IN WHICH MC9S12XDT512 WITH XGATE COPROCESSOR S IN BUILT. can i use same "CAN DRIVER"WHICH IS GIVEN IN AN2726.PDF......MEANS WHAT SHOULD I CAHNGE IN CAN DRIVER SOFTWARE FOR MC9S12XDT512... PLEASE HELP ME.........

ラベル(1)
0 件の賞賛
返信
1 返信

1,103件の閲覧回数
Alban
Senior Contributor II
Hello !
 
The AN2726 is written for the S12XDT512. You don't need to change the code.
You need to follow the guide to create the mailboxes you need.
Everything is explained is a lot in details in the AN2726.
 
The software is available with AN2726SW.
 
Alban.
 
AN2726SW Source files for AN2726 in ZIP format  FREESCALE  zip  155KB  Rev1  Released Date 3/23/2005  
0 件の賞賛
返信