DEMO9S121XXEP100 Setup file for Windows 7 64 bit operating system

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

DEMO9S121XXEP100 Setup file for Windows 7 64 bit operating system

959 Views
Drake
Contributor II

Demo board drivers will not load in a Windows 7 envorinment. Is there a 64 bit driver version available. My setup files are dated 6/22/2010.The computer suggests getting a 64 bit version software. Is this available? Otherwise is there a work-around for loading the demo software in Windows 7?

Labels (1)
0 Kudos
Reply
2 Replies

848 Views
Drake
Contributor II

I finally got around this by not using the program. I installed the USB Multilink BDM programmer and used the programmer to program and debug my demo board. The system was much more stable. I had to install a connector on the demo board.

0 Kudos
Reply

848 Views
Rodrigo_Cruz
Contributor I

you could use the DEMO board in Windows 7? which connector I have to put on the board?

0 Kudos
Reply