DC Motor control for S12ZVC

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

DC Motor control for S12ZVC

1,531件の閲覧回数
jtpark
Contributor IV

Hi,

 

I want to drive a position control of DC Motor for S12ZVC.

Would you provide to me an exam. code?

I have no idea.

 

Thanks.

ラベル(1)
0 件の賞賛
返信
1 返信

1,179件の閲覧回数
RadekS
NXP Employee
NXP Employee

Hi J.T.

I am afraid that your request is too simply and simultaneously too complex.

The S12ZVC do not have any special features for motor control (it is rather CAN node).

Did you mean S12ZVM family? The S12ZVM family contains FET drivers and other features for motor control.

http://www.nxp.com/products/software-and-tools/run-time-software/automotive-software-and-tools/motor...

http://www.nxp.com/products/automotive-products/microcontrollers-and-processors/16-bit-s12-magniv/3-...

The S12ZVH family for automotive instrument cluster solution contains four stepper motor drivers with stall detect.

http://www.nxp.com/products/automotive-products/microcontrollers-and-processors/16-bit-s12-magniv/s1...

Which type of motor you would like to use?

Brushed DC motor, Brushless DC (BLDC/PMSM) or Stepper motor?

Your motor will contain sensor or you plan sensorless solution?

What is supposed motor power?

If you want to use S12ZVC and drive Brushed DC motor, you will need some H-Bridge:

http://www.nxp.com/products/power-management/engine-and-dc-motor-control/h-bridges:PWRHBRIDGESTEPMTR

I would like to recommend for example MC33926 or new HB2001.


I hope it helps you.

Have a great day,
RadekS

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信