DBG trigger error

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

DBG trigger error

2,162件の閲覧回数
kdn
Contributor III

what is this DBG trigger error?

 

 

 

18428_18428.pngDBG trogger.png

ラベル(1)
タグ(3)
0 件の賞賛
返信
3 返答(返信)

1,971件の閲覧回数
iggi
NXP Employee
NXP Employee

Hi,

There can be many reasons to cause this - COP reset, Illegal instruction, Illegal memory access, etc.

For the trigger mode usage there are 4 modes: - Automatic, - Expert, - Profiling & Coverage, - Disable.

The default mode and the option we suggest to use is the Automatic mode. By this way the tool will manage automatically the trigger function.

More detailed information about the triggers you can find in S12(X) Debugger Manual, chapter 17 On-Chip DBG Module for S12, S12S, S12G, S12P, S12X Platforms"

S12(X) Debugger Manual

Regards,

iggi

0 件の賞賛
返信

1,971件の閲覧回数
kdn
Contributor III

How can i attache my project workshop to send you a mail

0 件の賞賛
返信

1,971件の閲覧回数
kdn
Contributor III

I  have used processes expert for CAN initialization. I am able to receiver CAN data and transmitter it successfully in polling mode, but when I am trying it in interrupt mode it's not working. please help me to configure it in interrupt mode.    

0 件の賞賛
返信