DBG trigger error

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

DBG trigger error

2,156 次查看
kdn
Contributor III

what is this DBG trigger error?

 

 

 

18428_18428.pngDBG trogger.png

标签 (1)
标记 (3)
0 项奖励
回复
3 回复数

1,965 次查看
iggi
NXP Employee
NXP Employee

Hi,

There can be many reasons to cause this - COP reset, Illegal instruction, Illegal memory access, etc.

For the trigger mode usage there are 4 modes: - Automatic, - Expert, - Profiling & Coverage, - Disable.

The default mode and the option we suggest to use is the Automatic mode. By this way the tool will manage automatically the trigger function.

More detailed information about the triggers you can find in S12(X) Debugger Manual, chapter 17 On-Chip DBG Module for S12, S12S, S12G, S12P, S12X Platforms"

S12(X) Debugger Manual

Regards,

iggi

0 项奖励
回复

1,965 次查看
kdn
Contributor III

How can i attache my project workshop to send you a mail

0 项奖励
回复

1,965 次查看
kdn
Contributor III

I  have used processes expert for CAN initialization. I am able to receiver CAN data and transmitter it successfully in polling mode, but when I am trying it in interrupt mode it's not working. please help me to configure it in interrupt mode.    

0 项奖励
回复