Custom BDM frogrammer for HCS12, S12X

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Custom BDM frogrammer for HCS12, S12X

2,293件の閲覧回数
Eric_t
Contributor III

Hello,

We are going to develop a custom BDM programmer for mc9s12dg256, mc9s12xdt512 and mc9s12xeq512 controllers.

Does anyone know if nxp give any schematics or/and software for a BDM programmer to use them as starting point?

Thank you

0 件の賞賛
返信
2 返答(返信)

2,285件の閲覧回数
lama
NXP TechSupport
NXP TechSupport

Hi,

Something interesting…you can use translator from Czech language..

https://vyvoj.hw.cz/teorie-a-praxe/konstrukce/opensourcebdm-jednoduchy-programator-pro-mikrokontrole...

or

http://usbdm.sourceforge.net/USBDM_V4.9/USBDM_JS16/html/

or

I also found one old folder in my PC (attached) but research is up to you.

BTW; why to invent already existing?   Effort and price of the development  lead me to www.pemicro.com usb bdm multilink. This interface together with hiwave.exe which is a part of CodeWarrior provides you programing of S19 files (for free) together with debuging possibilities if you use entire IDE. You can also buy programmer from pemicro.

 

Best regards,

Ladislav

0 件の賞賛
返信

2,258件の閲覧回数
Eric_t
Contributor III

Ηι,

We provide our customers with a box for calibration, testing, configuration and firmware update through the bootloader. Some older devices do not have a bootloader and we want to add a firmware update via the BDM port.

It is convenient for our customers to have an all-in-one box

0 件の賞賛
返信