Confused in my Program

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Confused in my Program

ソリューションへジャンプ
3,270件の閲覧回数
chowjun
Contributor I

 I want to use data flash in s12xs128 

 

void Dflash_Wt(uint paddr,unsigned dat){  while(FSTAT_CCIF == 0);       //Waiting Complete  FSTAT   = 0X30;               //Clear ACC PVI  FCCOBIX = 0;                  //step 0   FCCOBHI = 0X11;               //0X11  FCCOBLO = 0x10;               //D-FLASH block address  FCCOBIX = 1;                  //step 1  FCCOB   = paddr;              //Global Address Of Word To Be Program  FCCOBIX = 2;                  //step 2  FCCOB   = dat;                //Word 0 program value  FSTAT |=0X80;                 //lunch command  while(FSTAT_CCIF == 0);       //Waiting Complete}

paddr = 0;

dat    = 0x55;

 

after functoning this program  , the the word 0x55 can't be written , I look the address 0x100000 ,but it is empty.  I don't know which part of the code is wrong?

thanks!

ラベル(1)
0 件の賞賛
返信
1 解決策
1,901件の閲覧回数
nandu
Contributor III

Apart from the points mentioned by James, if you are using Codewarrior Compiler and the debugger is "True-Time Simulator & Real-Time Debugger", then right click on the "Memory" window and select the

"Adress  Space" option to 'Global'. In general this debugger sets this option as 'Logical'. So, this can be reason that you could not see any data at memory location, because debugger shows the logical address when the "Address Space" is selected as 'Logical'.

 

Hopes this helps

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
1,901件の閲覧回数
jsmcortina
Contributor III

Is the flash erased?

Have you initialised FCLKDIV ?

 

What bitsize is "unsigned" ?

 

Have you checked the assembly output?

 

James

0 件の賞賛
返信
1,902件の閲覧回数
nandu
Contributor III

Apart from the points mentioned by James, if you are using Codewarrior Compiler and the debugger is "True-Time Simulator & Real-Time Debugger", then right click on the "Memory" window and select the

"Adress  Space" option to 'Global'. In general this debugger sets this option as 'Logical'. So, this can be reason that you could not see any data at memory location, because debugger shows the logical address when the "Address Space" is selected as 'Logical'.

 

Hopes this helps

0 件の賞賛
返信
1,901件の閲覧回数
chowjun
Contributor I

Thanks for James and Nandu, I confiuse Logical with Global Space.

 

 

thanks

chowjun 

0 件の賞賛
返信