Colpits blocking cap value for MC9S12DP256

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Colpits blocking cap value for MC9S12DP256

ソリューションへジャンプ
1,901件の閲覧回数
kevinhuffman
Contributor I

Freescale recommends use of a blocking cap with the MC9S12DP256 Colpits clock circuit.  The cap blocks DC voltage between Extal and the crystal.  It is referred to as C11 in the Developer User's Guide (V2.05).  What is a recommended value for C11 if the device is using a 16 MHz crystal with 18 pF caps?  Apparently this cap is recommended to limit DC voltage applied to the crystal (thereby reducing crystal life expectancy) and minimizing startup issues.

ラベル(1)
0 件の賞賛
返信
1 解決策
1,832件の閲覧回数
kef
Specialist I

Impedance of 10nF cap at 16MHz is less than 1 Ohm...

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
1,832件の閲覧回数
kevinhuffman
Contributor I

Perfect.  Thanks for the reply.  The Freescale documentation refers back to the crystal manufacturer for the correct value of a blocking cap.  This cap value doesn't appear to be addressed on ay crystal datasheets that I looked at.  I'll proceed with the 10 nF and see what happens.

0 件の賞賛
返信
1,833件の閲覧回数
kef
Specialist I

Impedance of 10nF cap at 16MHz is less than 1 Ohm...

0 件の賞賛
返信