Cold test fail

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Cold test fail

3,771件の閲覧回数
ahnjoseph
Contributor III

Hi

1. Application : Automotive HVAC 260W BLDC controller(12zvm) 

2. Issue : Cold test fail 

3. Condition : -40 degree & Input volt swing (8V<-->40V)

 When I did test my BLDC controller in chamber be setup  -40 degree and input Volt swing 8<---16V

 DC Input change 8V to 16 V then that happen Desaturation Err but 16V to 8V is no problem  

 

Err condition temperature is changed by Bootstrap cap value (Please Ref, parts" C23" on circuit)

Desaturation Err is dependent (Please Ref below data)

   1. 220uF: -7`C

  1. 320uF : -25`c
  2. 470uF : -27`c
  3. 570uF : -30`c
  4. 690uF : -1`c

I had tried volt change with slop then it case is no problem 

 

Can you advise to me ?

I had update my circuit & Oscilloscope capture data  (Yellow : High side PWM / Blue : Current of DC power line)

 

0 件の賞賛
返信
1 返信

3,679件の閲覧回数
danielmartynek
NXP TechSupport
NXP TechSupport

Hi,

Have you tried adjusting GDU blanking time (GBKTIM2) and the desaturation levels (GDYDSLVL)?

Regards,

Daniel

0 件の賞賛
返信