Codewarrior - Reset ECU after Flashing

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Codewarrior - Reset ECU after Flashing

3,683件の閲覧回数
in-nitin-gupta
Contributor I

Hi

I am trying to add automation in my project execution. For the same, using the TCL scripts for flashing the binaries to the board. In order to bring the MCU in operation, currently need to reset the ECU externally. But looking for some option in the CodeWarrior IDE itself which can remove this manual intervention. 

Tried to explore the IDE. Found an option "Execute Reset" but somehow it is not working.

Looking for help.

0 件の賞賛
返信
5 返答(返信)

3,624件の閲覧回数
stanish
NXP Employee
NXP Employee

Hi,

Can you indicate:

1) which MCU are you targeting

2) which CodeWarrior version are you using

3) debug probe used to connect to your board

 

This will help to answer the question much faster.

BR.

Stan

0 件の賞賛
返信

3,587件の閲覧回数
in-nitin-gupta
Contributor I
MCU : MC9S12ZVLA128
Codewarrior Version : 10.6.4
Debugger : P&E Multilink USB
0 件の賞賛
返信

3,630件の閲覧回数
jiri_kral
NXP Employee
NXP Employee

Hi, 

did you try reset h command in TCL script? But it is possible that such command is not supported by your debug probe. More details you can find on page 39 in the guide which you shared in previous thread. 

0 件の賞賛
返信

2,998件の閲覧回数
in-nitin-gupta
Contributor I

reset h cmd is used for debugging session not flashing

0 件の賞賛
返信

3,587件の閲覧回数
in-nitin-gupta
Contributor I
Hey Jiri
as per document, reset h is used in debugging mode only whereas I am simply flashing my hardware using "Flash Programmer" utility in CodeWarrior
0 件の賞賛
返信