Can receiver、can module and error frame

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Can receiver、can module and error frame

2,221 次查看
allenlw
Contributor III

        If I enable the CAN receiver (like TJA1042), but not enable the corresponding CAN module that connect to this CAN receiver, then when I initiate a power on situation, there will appear some error frames.

        Can someone explain to me the specific reason why there are can error frames?

        Thanks a lot.

标签 (1)
0 项奖励
回复
2 回复数

2,123 次查看
RadekS
NXP Employee
NXP Employee

Hi,

Ideas:

When CAN module is enabled, the TX pin is setup as output and the pull device is disabled. The RX pin is setup as input and pull-down is disabled.
The log0 at TX pin means the dominant state while log1 is the recessive state.
So, it seems that TX pin your case has temporary/permanent log0 until you enable the CAN module.
Please check appropriate pins at the Pin Summary table in RM chapter 1 and focus mainly on reset state.
In the case of Off/Down state, you may need external pull-ups or GPIO initialization prior CAN transceiver enable.
Please check also your GPIO pin initialization code.

Additionally, the CAN module cannot acknowledge any CAN message on CAN bus prior to its own initialization.
So, if the second CAN node sends any data without acknowledging from MCU (or any other CAN node), it will lead to error passive/active frames on CAN bus until the second CAN node ends in the bus-off state.


I hope it helps you.

Have a great day,
Radek

0 项奖励
回复

2,123 次查看
allenlw
Contributor III

thanks for your answer

0 项奖励
回复