Can I run a FLASH write routine from FLASH?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Can I run a FLASH write routine from FLASH?

1,806 次查看
pederalm
Contributor II
Can I erase a part of flash with a program in FLASH? Or do I have to erase flash from a RAMprogram?
 
This is what I like to do:
 
I use the MC9S12XDP512 with 512k flash. I want to store data at page $E8-$EF (block 2, 128k). All other FLASH is for program code. Sometimes I would like to change the data located in block 2. Is it possible to do that with a FLASH routine executing from FLASH or do I have to change the data from a RAM routine? My idea is to have the FLASH routines in the unpaged FLASH area.
标签 (1)
0 项奖励
回复
1 回复

1,010 次查看
Steve
NXP Employee
NXP Employee
Yes, you can erase & program one flash block while running in another. You cannot erase or program the flash block in which you are running.
0 项奖励
回复