COP not working as expected

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

COP not working as expected

1,357 次查看
jberri
Contributor II

I am currently using an MC9S12E128 processor and I have a troublesome problem.  If I enable the COP and then move to a loop where I don't reset the COP, I am not vectoring to the

address placed in the "COP monitor fail reset vector" (0xFFFA).  Currently the location 0xFFFA has 0xC00C as the address.  At that address I sit in an endless loop flashing an LED if I don't reset the COP. 

 

I am using CodeWarrior 5.9.0 and when I am debugging the code the debugger stops at address 0x4A4D.  If I disconnect the debugger and do a power reset I never see the software locking up at the endless flashing LED loop, so it's not a debugger issue.

 

At this point I can't get the COP to pull a reset.  What could possibly be going wrong???

 

; code section

            ORG   $C000

Entry:     ldx    #$0500         ;Reset stack pointer

              txs

              ldaa   #$47           ;Enable COP

              staa   COPCTL

 

 

;Endless loop

_Startup:

           nop                  ;Don't reset COP

           bra  _Startup


;**************************************************************

;*                       COP TRAP                                    *

;**************************************************************

        

;COP vector address!!        

COPRes     equ   *

          

           ldaa  #$41       ;LED ON

           staa  PTM

           staa  DDRM

 

            ldx   #$FFFF

Decxs:  dex

            bne   Decxs

 

            ldaa  #$40        ;LED OFF

            staa  PTM

         

            ldx   #$FFFF

Decys:  dex

            bne   Decys

            bra   COPRes      ;Endless branch!!!               

标签 (1)
标记 (1)
0 项奖励
回复
2 回复数

1,155 次查看
iggi
NXP Employee
NXP Employee

Hi,

Do you use your custom made board? Or is it a Freescale one?

The reset line shouldn’t contain any capacitor (or just very small value like 10nF). Otherwise the COP reset can be recognized as a normal external reset and the vector 0xFFFE will be fetched.

The reason is following:

If the watchdog expires the reset line is forced to zero for 128 cycles and released then. The state of reset pin is checked after next 64 cycles. If the pin is in high state, then the source of reset is recognized as a COP. If the pin is still in low state, then it means that the pin is driven low externally – recognized as an external reset.

If the capacitor is connected then the rising edge is too slow and after 64 cycles the state of reset line can be recognized as a low level. This also says that the external reset signal has to be longer than 192 cycles.

 

The COP reset behavior is the same as POR reset – the stack pointer is not defined, all registers are in default states. So, the initialization has to be done again. The best way is to take care about critical events in the interrupt and then jump to the _startup routine and run the code like after POR reset.

But, looking in your code, there seems to be problem with the branch instruction i.e. bra _Startup.

In most cases, the jump assmbler instruction is used instead :

asm jmp _Startup;

The thing is that BRA instruction has offset of 256 (-128,127), so if the code is executed somewhere at 0xC000, there is no chance to branch to reset vector (0xFFFE).

Operation of BRA:

(PC) + $0002 + Rel ⇒ PC

Rel is a relative offset stored as a two’s complement number in the second byte of the branch instruction.

Regards,

iggi

0 项奖励
回复

1,155 次查看
kef2
Senior Contributor V

Quote from manual, which explains the issue:

  • RESET is an active low bidirectional control signal that acts as an input to initialize the MCU to a known

start-up state. It also acts as an open-drain output to indicate that an internal failure has been detected in

either the clock monitor or COP watchdog circuit. External circuitry connected to the RESET pin should

not include a large capacitance that would interfere with the ability of this signal to rise to a valid logic one

within 32 ECLK cycles after the low drive is released. Upon detection of any reset, an internal circuit

drives the RESET pin low and a clocked reset sequence controls when the MCU can begin normal

processing.

0 项奖励
回复