CCS Protocol Plugin: Unknown Protocol Error

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

CCS Protocol Plugin: Unknown Protocol Error

2,769 Views
ShreyasRaj
Contributor I
Hi,
I am using the MC56F8367 evaluation board for motor control. When i try to connect to the board through Code Warrior IDE, I get the error "CCS Protocol Plugin: Unknown Protocol Error". I had not got this error until last week. I went through the forum: http://forums.freescale.com/freescale/board/message?board.id=CWDSPCOMM&message.id=697&query.id=11033... and tried all the solutions posted on it and still the problem persists. The version of the IDE I use is 5.6.1.1658.

The log of the session says:

check_min_version(serverh=0,*version)
  api version: 00000004 00000005
config_chain(serverh=0,cc=0,count=1,*devlist,*generic)
  devlist: hawkv2
reset_to_debug(serverh=0,cc=0)
  ERROR(39): Subcore error encountered during multicore operation


Any help?

Thank you,
Shreyas


Message Edited by Shreyas Raj on 2008-11-03 09:54 AM
Labels (1)
0 Kudos
Reply
0 Replies