CAN can not send out data.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

CAN can not send out data.

1,665件の閲覧回数
100asong
Contributor I

Hi,Dear All

        I meet an strange thing:CAN can not send out data when I operate the flash.But if I don't operate the flash,I means I disable the flash code related, CAN can send normally out data .MCU is mc9s12xep100.

       When my CPU is running, CAN code is in flash zero,Flash code is in ram. The question is from here?

       Please give me support.Thanks!!!

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

1,238件の閲覧回数
Lundin
Senior Contributor IV

What does "operate the flash" mean? Are you writing to flash memory cells? Program memory flash or "data flash"?

If you are writing to program memory, no code in the flash bank being written to can be executed at the same time.

 

 

0 件の賞賛
返信

1,238件の閲覧回数
100asong
Contributor I

Dear sir

      

     I had slove this issue,it is caused by my code.And I debug it to find it.

0 件の賞賛
返信