CAN can not send out data.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

CAN can not send out data.

1,668 Views
100asong
Contributor I

Hi,Dear All

        I meet an strange thing:CAN can not send out data when I operate the flash.But if I don't operate the flash,I means I disable the flash code related, CAN can send normally out data .MCU is mc9s12xep100.

       When my CPU is running, CAN code is in flash zero,Flash code is in ram. The question is from here?

       Please give me support.Thanks!!!

Labels (1)
0 Kudos
Reply
2 Replies

1,241 Views
Lundin
Senior Contributor IV

What does "operate the flash" mean? Are you writing to flash memory cells? Program memory flash or "data flash"?

If you are writing to program memory, no code in the flash bank being written to can be executed at the same time.

 

 

0 Kudos
Reply

1,241 Views
100asong
Contributor I

Dear sir

      

     I had slove this issue,it is caused by my code.And I debug it to find it.

0 Kudos
Reply