CAN bus issue for 200 meters cable

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

CAN bus issue for 200 meters cable

Jump to solution
2,123 Views
aaronlee
Contributor V

Hi,

We use 10 boards(S12ZVCA) to send CAN message every 10 seconds. And 1 board(S12ZVCA) to collect those CAN message.

It can work fine in 10 meters cable. But it is unstable in 200 meters cable. How to solve the issue? Do you have any recommend?

Slew rate: 4

Baud rate: 250kbps

Time segment 1: 4 (We will try "12" on next Monday)

Time segment 2: 1

RSJ: 1

Sample per bit: 3 samples

BR, Aaron

FreescaleCAN_12,1,1.png

CANPHY.png

Labels (1)
1 Solution
2,020 Views
aaronlee
Contributor V

Hi Ladislav,

Thanks for your reply.

We only change Time segment 1 from 4 to 12. It can work stable in 200 meters cable.

The parameter as follow:

Slew rate: 4

Baud rate: 250kbps

Time segment 1: 12

Time segment 2: 1

RSJ: 1

Sample per bit: 3 samples

BR, Aaron

View solution in original post

0 Kudos
Reply
2 Replies
2,020 Views
lama
NXP TechSupport
NXP TechSupport

Hi,

The long transmission line has its own distributed parameters. They creates reactance which depends on frequency. Moreover, they deforms edges of signals.

 

So you can solve your issue:

Decrease bitrate

Do correct bitrate calculations including real propagation delays ( https://www.nxp.com/docs/en/application-note/AN1798.pdf )

Use wires with low R/L/C parameters.

Use some repeaters.

Wireless CAN

 

For this distance probably you could use RS485 and UART.

 

Best regards,

Ladislav

2,021 Views
aaronlee
Contributor V

Hi Ladislav,

Thanks for your reply.

We only change Time segment 1 from 4 to 12. It can work stable in 200 meters cable.

The parameter as follow:

Slew rate: 4

Baud rate: 250kbps

Time segment 1: 12

Time segment 2: 1

RSJ: 1

Sample per bit: 3 samples

BR, Aaron

0 Kudos
Reply