Bootloader CAN for S12Z

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Bootloader CAN for S12Z

1,828件の閲覧回数
giacomantonio_n
Contributor I

Hi,

I'm writing a bootloader for a S12ZVC microcontroller for flashing the firmware throught CAN bus. I see that in AN4723 - S12Z MagniV Bootloader Application Note, there is an example of bootloader with SCI protocol. There is an example on CAN protocol too?

Thank you,

Antonio

ラベル(1)
タグ(2)
0 件の賞賛
返信
1 返信

1,643件の閲覧回数
lama
NXP TechSupport
NXP TechSupport

Hi,

we are very sorry but we are not able to provide you CAN bootloader.

However, principles are the same. The only difference is that data goes via CAN.

We provide an Uart examples because there is simple connection to a PC and there is good amount of UART communication applications which are free.

Best regards,

Ladislav

0 件の賞賛
返信