BLDC sensorless motor control using sample code(S12ZVML-MINIBRD)

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

BLDC sensorless motor control using sample code(S12ZVML-MINIBRD)

1,870件の閲覧回数
whaleshark
Contributor I

Hello all.

I want to know how to calculate the parameter for proper paramter to normal working.

I am testing with an MTRCKTSPNZVM128 EV board.
In the S12zvml mini-brd sample code, bldc is referenced.

S12ZVML 3-phase BLDC/PMSM Evaluation Kit | NXP Semiconductors

I checked that the motor on the ev board is running, but it's not working on the target motor.
It flinches slightly with a whine, then stops when one of the 'Idcb HI', 'GDU', and 'Stall' errors occurs.
I suspect that it is because the parameter value in the sample code is different.

The target motor has 14 poles. And it is being developed at 500-25000 rpm.
So I'm going to test it while modifying the value, but I don't know how to calculate it. I'm asking if there's a calculation formula.

Below is the parameter in the sample code.

/***** High speed scaling *********************
 * For 4 pole-pairs motors
 * Boundary values for 1.28 us timer period:
 * - Minimal speed:        60 rpm
 * - Minimal speed scaled: 86
 * - Maximal speed:        22887 rpm
 * - Maximal speed scaled: 32767
 *********************************************/
#define SPEED_CALC_NUMERATOR            16777216
#define STALLCHECK_MIN_CMT_PERIOD       97          // 97 = 125 us (20 krpm on 4 pole-pairs motor), min value = 85 (22.89 krpm)
#define REQUIRED_RUN_SPEED              (1432*2)    // 2000 rpm
// 1431.655765 = 1000 rpm
#define MIN_SPEED                       (1432/2)    // 500 rpm minimal speed for Down button control (should be min 10% of nominal motor speed)
#define MAX_SPEED                       (1432*5)    // 5 krpm maximum speed for Up button control
#define SPEED_STEP                      FRAC16(100.0/22887.0)   // 100 rpm, Up/Down step for button controls
#define BTN_PERIOD_DIVIDER              100     // scan buttons every 0.1 s only
//*****
0 件の賞賛
返信
1 返信

1,828件の閲覧回数
RadekS
NXP Employee
NXP Employee

Dear whaleshark,

Please look at detailed answer here: https://community.nxp.com/t5/S12-MagniV-Microcontrollers/BLDC-Motors-param/m-p/700945#M14540

I hope it helps you.

 

Best regards

RadekS

0 件の賞賛
返信