BLDC PMF problem

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

BLDC PMF problem

1,400件の閲覧回数
bskim
Contributor I

hello everyone 

im using MCU 12zvmc256 model

i made 3 controller boards to control BLDC motor

tried operating one board and confirmed that the trapezoidal back-emp appears normally.

However, in the other boards of the same circuit, PMF V High gate not Output. 

Also, the AMP[0](Current Sensing) ADC Voltage fluctuates by 500mV. IS The MCU bad?

 

0 件の賞賛
返信
1 返信

1,376件の閲覧回数
danielmartynek
NXP TechSupport
NXP TechSupport

Hello @bskim,

Do you see any GDU or PMF error flags?

GDU Flag Register (GDUF)

GDU Desaturation Error Flag Register (GDUDSE)

PMF Fault Enable Register (PMFFEN)

PMF Fault Interrupt Flag Register (PMFFIF)

 

Table below lists GDU faults and the corresponding action on the drivers.

danielmartynek_0-1651046594204.png

 

Regards,

Daniel

0 件の賞賛
返信