BLDC PMF problem

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

BLDC PMF problem

1,457 Views
bskim
Contributor I

hello everyone 

im using MCU 12zvmc256 model

i made 3 controller boards to control BLDC motor

tried operating one board and confirmed that the trapezoidal back-emp appears normally.

However, in the other boards of the same circuit, PMF V High gate not Output. 

Also, the AMP[0](Current Sensing) ADC Voltage fluctuates by 500mV. IS The MCU bad?

 

0 Kudos
Reply
1 Reply

1,433 Views
danielmartynek
NXP TechSupport
NXP TechSupport

Hello @bskim,

Do you see any GDU or PMF error flags?

GDU Flag Register (GDUF)

GDU Desaturation Error Flag Register (GDUDSE)

PMF Fault Enable Register (PMFFEN)

PMF Fault Interrupt Flag Register (PMFFIF)

 

Table below lists GDU faults and the corresponding action on the drivers.

danielmartynek_0-1651046594204.png

 

Regards,

Daniel

0 Kudos
Reply