Affect to performance of MCU

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Affect to performance of MCU

1,743 次查看
jtpark
Contributor IV

Hello.

 

Application is gateway of BCM.

According to datasheet of S912XDP512MAL, It has 5ch(CAN) of MCU.

I'd like to use 4ch. with high speed(500kbps).

Does it affect to performance of MCU?

标签 (1)
6 回复数

1,449 次查看
iggi
NXP Employee
NXP Employee

Hi,

well, it is logical that the number of peripherals used affect the MCU (i.e. CPU) performance.

Higher the number of peripherals, higher the performance, which means more current draw i.e. more power consumption.

You can check the MC9S12XDP512 datasheet where the Appendix A.1.10 provides supply currents for several peripheral sets (Table A-10. Run and Wait Current Characteristics).

Regards,

iggi

0 项奖励
回复

1,449 次查看
jtpark
Contributor IV

Thanks for your reply.

I meant overload of MCU, not power consumption.

When I used to gateway in MC9S12XDP512, I worry about overload of MCU.

Thanks.

0 项奖励
回复

1,449 次查看
iggi
NXP Employee
NXP Employee

I don't think you will overload the MCU with 5-channel CAN. You should use a co-processor - the XGATE which is used to handle data transfers between peripherals and internal memory. Therefore the main core interrupt load would be lowered. The peripheral interrupts should be handled by XGATE.

Also the MCU load depends on how many other peripherals you use in the application, but in the end it's hard to believe it will be overloaded. Anyhow, you should perform some tests.

regards,

iggi

0 项奖励
回复

1,449 次查看
jtpark
Contributor IV

Thanks.

I use only 4channel CAN Interface for gateway. I don't use ohter peripheral.

In this case, does it cause overload of MCU ?

regards,

JT Park.

0 项奖励
回复

1,449 次查看
iggi
NXP Employee
NXP Employee

No, it would not cause the MCU overload.

1,449 次查看
jtpark
Contributor IV

Thanks for your reply.

regards,

JT Park

0 项奖励
回复