Accessing paged RAM from XGATE - S12XEQ384

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Accessing paged RAM from XGATE - S12XEQ384

2,546 Views
saravanakumar_m
Contributor I

Hi,

 

i am using a S12XEQ384 with 24 kB RAM. I initially linked XGATE data to unpaged RAM. Later due to certain reasons i need to move it to paged RAM. Since then the cpu application code never runs and always an XGATE access violation occurs. 

 

here is a section of my prm file:

 

     //RAM_XGATE_STK = READ_WRITE  0xFA1000 TO 0xFA10FF ALIGN 2 [1:1]; /* The stack is set by the XGATE compiler option -Cstv=A100 */
      RAM_XGATE_DATA= READ_WRITE  0xFA1100 TO 0xFA12FF ALIGN 2 [1:1]; /* word align for XGATE accesses */
     
      RAM_FA        = READ_WRITE  0xFA1300 TO 0xFA1FFF; // ALIGN 2[1:1]; /* is also mapped to XGATE:  0xA000..0xAFFF */
      RAM_FB        = READ_WRITE  0xFB1000 TO 0xFB1FFF;
      RAM_FC        = READ_WRITE  0xFC1000 TO 0xFC1FFF;
      RAM_FD        = READ_WRITE  0xFD1000 TO 0xFD1FFF;
/*    RAM_FE        = READ_WRITE  0xFE1000 TO 0xFE1FFF; intentionally not defined: equivalent to RAM: 0x2000..0x2FFF */
/*    RAM_FF        = READ_WRITE  0xFF1000 TO 0xFF1FFF; intentionally not defined: equivalent to RAM: 0x3000..0x3FFF */

 

Can someone help on this ?

 

Thanks,

Saravana

 

Added p/n to subject.

Message Edited by NLFSJ on 2009-07-02 12:57 PM
Labels (1)
0 Kudos
Reply
2 Replies

1,435 Views
CompilerGuru
NXP Employee
NXP Employee

The main different in between paged and unpaged is for the S12, is the data shared in between the cores?

Also how does it fail, does any code get executed for the XGATE at all?

How is the code for the XGATE mapped, flash?

Is the XGATE stack properly initialized?

 

I did not notice anything special from the provided information, I would think we need more hints on what is going on. With a bdm it should not be too hard to see what fails.

 

Daniel

0 Kudos
Reply

1,435 Views
jsmcortina
Contributor III

Have you confirmed that your code is getting copied to the right region of memory?

 

Do the XGATE interrupt vectors point to the right address?

 

James

0 Kudos
Reply