ATD Data Collection - EVB9S12XEP100 .

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

ATD Data Collection - EVB9S12XEP100 .

2,371 Views
Nicklop
Contributor I
Hi,
 
I am using EVB9S12XEP100 evaluation board. Now I am doing a task on measuring the analog signal using the internal ATD of MCU9S12XEP100. Is there any method that I can use to pull the converted data I get from ATD into the computer, especially into the Code Warrior? If there are, then how?
 
Is it possible to store the converted data into a text file or plot into the graph straight forward after the data is received from ATD?
 
 
 
 
 
Added p/n to subject.


Message Edited by NLFSJ on 2008-06-12 06:01 AM
Labels (1)
0 Kudos
Reply
2 Replies

1,459 Views
allawtterb
Contributor IV
If you want something that is already setup to do the graphing of the data I would suggest taking a look at FreeMASTER provided which can be downloaded here:
 
 
I have not used it extensively, but I found it very handy for quick debugging of variables in real time.  Depending ont the sample rate you need, FreeMASTER's quick setup using the BDM might be just what you need.  It provides a facility for saving the sampled data to a text file through the BDM as well displaying directly in a very nice graphing utility with optional auto-scaling.  
0 Kudos
Reply

1,459 Views
Nicklop
Contributor I
Is there possible to do the graphing using the visualization tool of Code Warrior?
 
Why the real-time debugger becomes very unstable and always hang at there when I do the debugging on board?


Message Edited by Nicklop on 2008-06-13 03:21 AM
0 Kudos
Reply