ADC intialization of MC9s12zvml128 controller

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

ADC intialization of MC9s12zvml128 controller

1,090 Views
beenu
Contributor I

ADC intialization for MC9s12zvml128 controller is giving a problem. The result register ADCRBP is being loaded with the given address. where as ADCCBP is properly being loaded. What could be the problem?

Labels (1)
0 Kudos
Reply
1 Reply

844 Views
ankur_kala
NXP Employee
NXP Employee

Hi,

to go through the various peripheral initialization in case of S12ZVM, you can go through the motor control application code shared at freescale webpage -- MTRCKTSBNZVM128: 3-phase Sensorless BLDC Development Kit with S12 MagniV MC9S12ZVML128 MCU

0 Kudos
Reply