A problem about the algorithm of S-type acceleration and deceleration

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

A problem about the algorithm of S-type acceleration and deceleration

ソリューションへジャンプ
2,754件の閲覧回数
maxxu
Contributor IV

Hi

   Hello everyone, I am currently designing a BLDC driver based on position control。

   I use function the  libraries ,MC9S12ZVM_AMMCLIB_RTM_1_1_23_BIN.

   Is there a function or reference design for T-type acceleration / deceleration or S-type acceleration / deceleration

    Thank you very much

タグ(1)
0 件の賞賛
返信
1 解決策
2,730件の閲覧回数
pachamatej
NXP Employee
NXP Employee

Hello,

There is no such a function in the library yet, however, you can create one using basic blocks (e.g. two integrators in series with look-up tables of input jerk / acceleration limit, or, square root function directly).

Best regards,

Matej

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
2,731件の閲覧回数
pachamatej
NXP Employee
NXP Employee

Hello,

There is no such a function in the library yet, however, you can create one using basic blocks (e.g. two integrators in series with look-up tables of input jerk / acceleration limit, or, square root function directly).

Best regards,

Matej

0 件の賞賛
返信