9sdp256 vs 9sdt256

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

9sdp256 vs 9sdt256

2,287 Views
untel
Contributor I

Can somone tell me the exact  difference between the 9sdp256 and 9sdt256. Are they interchanable?

They both have the same datasheet. What should I search for in the datasheet?

Is there any cross reference chart avaliable ?

Thanks helping.

Untel.

Labels (1)
0 Kudos
Reply
4 Replies

1,919 Views
kef
Specialist I

You should search in the datasheet for derivative differencies. DP has 5 MSCAN modules and J1850/BDLC. DT - 3 MSCAN's (CAN0, CAN1, CAN4) and no J1850/BDLC.

0 Kudos
Reply

1,919 Views
Lundin
Senior Contributor IV

Also, early versions of DP256 which can be found on evaluation boards are full of nasty silicon bugs. If you buy an evaluation board with a DP256 on it, make sure to replace the chip with the most up-to-date mask set and read all erratas carefully.

 

If you plan to use DT256 in production, you may as well put that chip on instead, they are pin compatible.

0 Kudos
Reply

1,919 Views
Eric_t
Contributor III

Also, early versions of DP256 which can be found on evaluation boards are full of nasty silicon bugs!!!!

 

I have severe problems with electrostatic discharge with DG256; I apply 8KV air discharge and controller resets. Do you know if early versions of DG256 have problems with electrostatic discharge?

 

Best Regards

Nikos

0 Kudos
Reply

1,919 Views
Lundin
Senior Contributor IV

Nope, the silicon bugs are related to behavior of peripherals. As far as I know, even the earliest DP256 went through quite tough automotive qualifications EMI- and ESD-wise. It sounds very much like a board design problem to me.

 

However, let us not hi-jack this post for that discussion.

 

0 Kudos
Reply