9S12XEP100 with a simple RTI initialization

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

9S12XEP100 with a simple RTI initialization

跳至解决方案
1,195 次查看
nocturnalHippoz
Contributor I

Hi everyone,

 

I'm having a bit of a problem with initializating the RTI on the 9S12XEP100 chip. Enclosed with this Email is a copy of the code. The error that I'm receiving during compiling is:

 

"L1907: Fixup overflow in_Vector_7, to rti_isr type 1, at offset 0x0"

 

At first, I thought I was addressing off the wrong vector address but opening the the vector map in the .h file shows that the Vrti is at 7. Does anyone have any ideas or recommendations? Thank you in advance.

 

Sincerely,

Ron.

标签 (1)
0 项奖励
回复
1 解答
1,015 次查看
CompilerGuru
NXP Employee
NXP Employee

Interrupt handlers must be explicitely allocates in NON_BANKED in the banked memory model.

 

Search for NON_BANKED and interrupt in the forum, e.g. here is a sample use, there are many others:

 

https://community.freescale.com/message/73150#73150

 

Daniel

在原帖中查看解决方案

0 项奖励
回复
2 回复数
1,016 次查看
CompilerGuru
NXP Employee
NXP Employee

Interrupt handlers must be explicitely allocates in NON_BANKED in the banked memory model.

 

Search for NON_BANKED and interrupt in the forum, e.g. here is a sample use, there are many others:

 

https://community.freescale.com/message/73150#73150

 

Daniel

0 项奖励
回复
1,015 次查看
nocturnalHippoz
Contributor I

Thank you! :smileyhappy:

0 项奖励
回复