9S12XDP512 - Spurious interrupt

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

9S12XDP512 - Spurious interrupt

2,425件の閲覧回数
Ermin
Contributor I

Hi,

I'm have a problem with spurious interrupt in a 9S12XDP512 processor.

I have two interrupts that some times occurs at the same time (XINT and PIT1).

Looking with the scope I realized that when they occur at the same time XINT ISR is runned and the PIT1 ISR gives me a spurious interrupt.

What can I do to make the processor run the PIT1 ISR after it ends the XINT ISR?

--
Alban Edit: Part number in subject line.

Message Edited by Alban on 2007-03-26 01:18 PM

ラベル(1)
0 件の賞賛
返信
1 返信

1,197件の閲覧回数
StephenRussell
Contributor I
What should happen is the XINT interrupt should be called by the hardware and set the I bit in the CCR.  This will prevent all maskable interrupts.  The XINT ISR should end with a rti instruction which will restore the previous state of the CCR.  If the I bit was clear before the XINT interrupt, it should now be clear, and the PIT1 interrupt should be taken.
 
You should be able to monitor the state of the I bit through this process by placing breakpoints.
 
Are you clearing the I bit in your startup code to enable interrupts?
0 件の賞賛
返信