9S12XDP512 BDM debug problem

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

9S12XDP512 BDM debug problem

4,878件の閲覧回数
sfb
Contributor I
Hello,
I am working with 9S12XDP512 and when connected to BDM there are some warnings and errors on debug screen. I checked the pins and see that :
VDD1 : 2.5V
VDD2 : 2.5V
VDDX2 : 5V
XCLKS : 5V (pulled high)
BKGD : 5V (pulled high)
VDDR1 : 5V
RESET : 5V (pulled high)
TEST : GND
VDDR2 : 5V
VDDA, VRH : 5V
VREGEN : 5V (pulled high)
VDDX1 : 5V
 
I see these warnings one ofter another:
first : "Loading a new application will stop the exacution of the current one"
and second : "Error Elf Loader
                       Error while writing to FFFE ... 101FE"
 
and last : "Failed to load
                 "C:\ ..... \P&E_Multilink_CyclonePro.abs"
 
And after all of these processor doesn't work. Why?
ラベル(1)
0 件の賞賛
返信
5 返答(返信)

2,864件の閲覧回数
stevo10
Contributor I
Hello,

Could it be the case the device is secured? Have you tried an unsecure script on the device?

Regards,

Stevo
0 件の賞賛
返信

2,864件の閲覧回数
sfb
Contributor I
Yes, I tried it but nothing changed.
0 件の賞賛
返信

2,864件の閲覧回数
JimDon
Senior Contributor III
First "Loading a new application will stop the execution of the current one" is just a warning, and can be turned off on one of the config panels - Detect target is running or something like that.

Tried "it" - tried what - did you down load P&E Unsecure and run it ?
0 件の賞賛
返信

2,864件の閲覧回数
sfb
Contributor I
No I didn't download anything for unsecure process, I did it from debugger menu.
But I see another thing:
I am using expanded mode MODC = 1, MODB = 0, MODA = 1 (1 is pull up and 0 is pulled low). And PK7 is high. When I remove the pull up resistor from MODA pin processor is running. Can someone explain me what is wrong with selecting Normal Expanded Mode like above hardware configuration (Because I think that there is a problem when starting Normal Expanded Mode and there is no problem for Normal Single Chip Mode)?
 
Best regards
0 件の賞賛
返信

2,864件の閲覧回数
kef
Specialist I
Debuggers normally expect target being configured for normal single chip mode. MODC(BGND) pulled high, MODA and MODB pulled low. MODC:MODB:MODA=100.
To get into active background mode (special single chip mode), debugger pulls MODC low and pulses reset low. Target gets reset into special single chip mode, 000.
 
Now, if your target is set for normal expanded, 101, then hitting connect in debugger will also make MODC pulled low and target will be reset. Thats mode 001, Emulation Single Chip. I guess it's not what you want.
 
I think you need to jumper your target for normal single chip and enable expanded memory at runtime. You may also try using hot-plugging mode, check hiwave->P&E multilink settings.
0 件の賞賛
返信