9S12X RAM data unreadable after function call

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

9S12X RAM data unreadable after function call

跳至解决方案
8,329 次查看
leroy_o
Contributor III

Hello,

 

I use the 9S12XEQ384 derivative. My compiling options are: -CPUHCS12XE -D__NO_FLOAT__ -D__MAP_FLASH__ -D__FAR_DATA -Mb -MapFlash -Onf -OnB=b -PSegObj

 

I first set an array of 8 bytes of data in func1.

Then I call func2 with a pointer to this array of 8 bytes as argument.

Inside func2, all data read from this array are 0s,I don't understand this.

 

I.e. the following program:

 

void func1_every1ms(void)

{

   U8 buffer[8] = {0, 0, 0, 0, 0, 0x0A, 0x0F, 0x05};

 

   log_printf("Inside func1, before call:\n");

   log_U32((U32)buffer);

   log_U32(*(U32 *)&buffer[0]);

   log_U32(*(U32 *)&buffer[4]);

 

   func2_handler(buffer);

 

   log_printf("Inside func1, after call:\n");

   log_U32(*(U32 *)&buffer[0]);

   log_U32(*(U32 *)&buffer[4]);

}

 

void func2_handler(U8 *buffer)

{

   if (buffer != NULL))

   {

   log_printf("Inside func2:\n");

   log_U32((U32)buffer));

   log_U32(*(U32 *)&buffer[0]);

   log_U32(*(U32 *)&buffer[4]);

   }

 

gives the following result:


Inside func1, before call

01B9C00

00000000

00000AF5

Inside func2:

01B9C00

00000000

00000000

Inside func1, after call

00000000

00000AF5


Does anyone have an idea why it is not possible to read back the 8 byte array of data inside func2, and why instead I read all zeros?

标签 (1)
标记 (4)
0 项奖励
回复
1 解答
7,778 次查看
kef
Specialist I

But you can reproduce problem in new project with IP sensitive things removed. If you can't reproduce the problem in small new project, then looking for differences should reveal what's wrong. Unfortunately it is very common to be lazy like a hell to not start new small experimental projects. People prefer spending hours looking at thousand of lines without any progress.

在原帖中查看解决方案

0 项奖励
回复
12 回复数
7,778 次查看
ZhangJennie
NXP TechSupport
NXP TechSupport

can you please upload your entire sample project folder in zip format to us thus we can check it directly? thanks!

0 项奖励
回复
7,778 次查看
leroy_o
Contributor III

This is an automotive company project, sorry I cannot publish it.

0 项奖励
回复
7,779 次查看
kef
Specialist I

But you can reproduce problem in new project with IP sensitive things removed. If you can't reproduce the problem in small new project, then looking for differences should reveal what's wrong. Unfortunately it is very common to be lazy like a hell to not start new small experimental projects. People prefer spending hours looking at thousand of lines without any progress.

0 项奖励
回复
7,778 次查看
leroy_o
Contributor III

Thanks for your recommandation to build a small projet.

My fault: there was a "switch" with 3 "cases" in func2_handler(); and I forgot the "break" instructions.

This caused the buffer not to be consistent.

Thanks again for having helped me.

0 项奖励
回复
7,778 次查看
leroy_o
Contributor III

added since last post:

The value of the pointer should read: 00001B9C, which is not unpagined RAM (0x2000 TO   0x3FFF).

How is such thing possible? Thanks for your answer.

0 项奖励
回复
7,778 次查看
kef
Specialist I

Either your PRM file is misedited or it is a result of allocating enormously big objects on the stack. Your buffer[] is allocated on stack. You should check, maybe some very big array is allocated on stack.

void func1_every1ms(void)

{

   U8 buffer[8] = {0, 0, 0, 0, 0, 0x0A, 0x0F, 0x05};

0 项奖励
回复
7,778 次查看
leroy_o
Contributor III

Ok, there was a typo:

void func1_every1ms(void)

{

   U8 buffer[8] = {0, 0, 0, 0, 0, 0, 0x0A, 0xF5};


The stack size is 0xBB8.


Here is the prm file:


/* This is a linker parameter file for the MC9S12XEQ384 */


/*

   This parameter file is setup in a generic way to allow exploring most common features of both cores:

   - S12X core

   - XGATE code and constants in FLASH and/or RAM

   - XGATE data and stack in RAM

   It might be required to adapt some of the definitions to best match your application.

*/

NAMES

    /* CodeWarrior will pass all the needed files to the linker by command line. But here you may add your additional files */

END

SEGMENTS /* here all RAM/ROM areas of the device are listed. Used in PLACEMENT below. All addresses are 'logical' */

/* Register space  */

/*    IO_SEG        = PAGED         0x0000 TO   0x07FF; intentionally not defined */

/* non-paged EEPROM */

      EEPROM        = READ_ONLY   DATA_NEAR IBCC_NEAR  0x0C00 TO   0x0FFF;

/* non-paged RAM */

      RAM           = READ_WRITE  DATA_NEAR            0x2000 TO   0x3FFF ALIGN 2[1:1]; /* word align for XGATE accesses */

/* non-banked FLASH */

      ROM_4000      = READ_ONLY   DATA_NEAR IBCC_NEAR 0x4000 TO   0x7FFB; /* instead of default 0x7FFF (see EGV PR 386) */

      ROM_C000      = READ_ONLY   DATA_NEAR IBCC_NEAR  0xC000 TO   0xCFFF;

      ROM_D000      = READ_ONLY     0xD000 TO   0xFEFB; /* instead of default 0xFEFF */

/*    VECTORS       = READ_ONLY     0xFF00 TO   0xFFFF; intentionally not defined: used for VECTOR commands below */

    //OSVECTORS     = READ_ONLY     0xFF10 TO   0xFFFF;  /* OSEK interrupt vectors (use your vector.o) */

/* paged EEPROM                     0x0800 TO   0x0BFF; addressed through EPAGE */

      EEPROM_00     = READ_ONLY   DATA_FAR IBCC_FAR  0x000800 TO 0x000BFF;

      EEPROM_01     = READ_ONLY   DATA_FAR IBCC_FAR  0x010800 TO 0x010BFF;

      EEPROM_02     = READ_ONLY   DATA_FAR IBCC_FAR  0x020800 TO 0x020BFF;

      EEPROM_03     = READ_ONLY   DATA_FAR IBCC_FAR  0x030800 TO 0x030BFF;

      EEPROM_04     = READ_ONLY   DATA_FAR IBCC_FAR  0x040800 TO 0x040BFF;

      EEPROM_05     = READ_ONLY   DATA_FAR IBCC_FAR  0x050800 TO 0x050BFF;

      EEPROM_06     = READ_ONLY   DATA_FAR IBCC_FAR  0x060800 TO 0x060BFF;

      EEPROM_07     = READ_ONLY   DATA_FAR IBCC_FAR  0x070800 TO 0x070BFF;

      EEPROM_08     = READ_ONLY   DATA_FAR IBCC_FAR  0x080800 TO 0x080BFF;

      EEPROM_09     = READ_ONLY   DATA_FAR IBCC_FAR  0x090800 TO 0x090BFF;

      EEPROM_0A     = READ_ONLY   DATA_FAR IBCC_FAR  0x0A0800 TO 0x0A0BFF;

      EEPROM_0B     = READ_ONLY   DATA_FAR IBCC_FAR  0x0B0800 TO 0x0B0BFF;

      EEPROM_0C     = READ_ONLY   DATA_FAR IBCC_FAR  0x0C0800 TO 0x0C0BFF;

      EEPROM_0D     = READ_ONLY   DATA_FAR IBCC_FAR  0x0D0800 TO 0x0D0BFF;

      EEPROM_0E     = READ_ONLY   DATA_FAR IBCC_FAR  0x0E0800 TO 0x0E0BFF;

      EEPROM_0F     = READ_ONLY   DATA_FAR IBCC_FAR  0x0F0800 TO 0x0F0BFF;

      EEPROM_10     = READ_ONLY   DATA_FAR IBCC_FAR  0x100800 TO 0x100BFF;

      EEPROM_11     = READ_ONLY   DATA_FAR IBCC_FAR  0x110800 TO 0x110BFF;

      EEPROM_12     = READ_ONLY   DATA_FAR IBCC_FAR  0x120800 TO 0x120BFF;

      EEPROM_13     = READ_ONLY   DATA_FAR IBCC_FAR  0x130800 TO 0x130BFF;

      EEPROM_14     = READ_ONLY   DATA_FAR IBCC_FAR  0x140800 TO 0x140BFF;

      EEPROM_15     = READ_ONLY   DATA_FAR IBCC_FAR  0x150800 TO 0x150BFF;

      EEPROM_16     = READ_ONLY   DATA_FAR IBCC_FAR  0x160800 TO 0x160BFF;

      EEPROM_17     = READ_ONLY   DATA_FAR IBCC_FAR  0x170800 TO 0x170BFF;

      EEPROM_18     = READ_ONLY   DATA_FAR IBCC_FAR  0x180800 TO 0x180BFF;

      EEPROM_19     = READ_ONLY   DATA_FAR IBCC_FAR  0x190800 TO 0x190BFF;

      EEPROM_1A     = READ_ONLY   DATA_FAR IBCC_FAR  0x1A0800 TO 0x1A0BFF;

      EEPROM_1B     = READ_ONLY   DATA_FAR IBCC_FAR  0x1B0800 TO 0x1B0BFF;

      EEPROM_1C     = READ_ONLY   DATA_FAR IBCC_FAR  0x1C0800 TO 0x1C0BFF;

      EEPROM_1D     = READ_ONLY   DATA_FAR IBCC_FAR  0x1D0800 TO 0x1D0BFF;

      EEPROM_1E     = READ_ONLY   DATA_FAR IBCC_FAR  0x1E0800 TO 0x1E0BFF;

      EEPROM_1F     = READ_ONLY   DATA_FAR IBCC_FAR  0x1F0800 TO 0x1F0BFF;

      EEPROM_FC     = READ_ONLY   DATA_FAR IBCC_FAR  0xFC0800 TO 0xFC0BFF;

      EEPROM_FD     = READ_ONLY   DATA_FAR IBCC_FAR  0xFD0800 TO 0xFD0BFF;

      EEPROM_FE     = READ_ONLY   DATA_FAR IBCC_FAR  0xFE0800 TO 0xFE0BFF;

/*    EEPROM_FF     = READ_ONLY                      0xFF0800 TO 0xFF0BFF; intentionally not defined: equivalent to EEPROM */

/* paged RAM:                       0x1000 TO   0x1FFF; addressed through RPAGE */

      RAM_XGATE_STK_L_ = NO_INIT  DATA_FAR           0xFA1000 TO 0xFA107D;

      RAM_XGATE_STK_L = NO_INIT   DATA_FAR           0xFA107E TO 0xFA107F;

      RAM_XGATE_STK_H_ = NO_INIT  DATA_FAR           0xFA1080 TO 0xFA10FD;

      RAM_XGATE_STK_H = NO_INIT   DATA_FAR           0xFA10FE TO 0xFA10FF;

      RAM_FA        = READ_WRITE  DATA_FAR           0xFA1100 TO 0xFA1FFF ALIGN 2[1:1]; /* is also mapped to XGATE:  0xA100..0xAFFF */

      RAM_FB        = READ_WRITE  DATA_FAR           0xFB1000 TO 0xFB1FFF ALIGN 2[1:1]; /* is also mapped to XGATE:  0xB000..0xBFFF */

      RAM_FC        = READ_WRITE  DATA_FAR           0xFC1000 TO 0xFC1FFF ALIGN 2[1:1]; /* is also mapped to XGATE:  0xC000..0xCFFF */

      RAM_FD        = READ_WRITE  DATA_FAR           0xFD1000 TO 0xFD1FFF ALIGN 2[1:1]; /* is also mapped to XGATE:  0xD000..0xDFFF */

/*    RAM_FE        = READ_WRITE  0xFE1000 TO 0xFE1FFF; intentionally not defined: equivalent to RAM: 0x2000..0x2FFF */

/*    RAM_FF        = READ_WRITE  0xFF1000 TO 0xFF1FFF; intentionally not defined: equivalent to RAM: 0x3000..0x3FFF */

/* paged FLASH:                     0x8000 TO   0xBFFF; addressed through PPAGE */

      PAGE_E0_0     = READ_ONLY   DATA_FAR IBCC_FAR  0xE08000 TO 0xE087FF; /* cannot be mapped to XGATE; XGATE sees registers here */

      PAGE_E0       = READ_ONLY   DATA_FAR IBCC_FAR  0xE08800 TO 0xE0BFFF ALIGN 2[1:1]; /* is also mapped to XGATE:  0x0800..0x3FFF        */

      PAGE_E1       = READ_ONLY   DATA_FAR IBCC_FAR  0xE18000 TO 0xE1BFFF ALIGN 2[1:1]; /* is also mapped to XGATE:  0x4000..0x7FFF        */

      // cannot be mapped to XGATE; this module should NOT be used for HC12 code when also used for XGATE code since

      //the HC12 will have priority over the XGATE accessing the FLASH modules resulting very poor performance of

      //the XGATE: Check allocation of this ranges in PLACEMENT below!

      PAGE_E2       = READ_ONLY   DATA_FAR IBCC_FAR  0xE28000 TO 0xE2BFFF;

      PAGE_E3       = READ_ONLY   DATA_FAR IBCC_FAR  0xE38000 TO 0xE3BFFF;

      PAGE_E4       = READ_ONLY   DATA_FAR IBCC_FAR  0xE48000 TO 0xE4BFFF;

      PAGE_E5       = READ_ONLY   DATA_FAR IBCC_FAR  0xE58000 TO 0xE5BFFF;

      PAGE_E6       = READ_ONLY   DATA_FAR IBCC_FAR  0xE68000 TO 0xE6BFFF;

      PAGE_E7       = READ_ONLY   DATA_FAR IBCC_FAR  0xE78000 TO 0xE7BFFF;

      PAGE_F0       = READ_ONLY   DATA_FAR IBCC_FAR  0xF08000 TO 0xF0BFFF;

      PAGE_F1       = READ_ONLY   DATA_FAR IBCC_FAR  0xF18000 TO 0xF1BFFF;

      PAGE_F2       = READ_ONLY   DATA_FAR IBCC_FAR  0xF28000 TO 0xF2BFFF;

      PAGE_F3       = READ_ONLY   DATA_FAR IBCC_FAR  0xF38000 TO 0xF3BFFF;

      PAGE_F4       = READ_ONLY   DATA_FAR IBCC_FAR  0xF48000 TO 0xF4BFFF;

      PAGE_F5       = READ_ONLY   DATA_FAR IBCC_FAR  0xF58000 TO 0xF5BFFF;

      PAGE_F6       = READ_ONLY   DATA_FAR IBCC_FAR  0xF68000 TO 0xF6BFFF;

      PAGE_F7       = READ_ONLY   DATA_FAR IBCC_FAR  0xF78000 TO 0xF7BFFF;

      PAGE_F8       = READ_ONLY   DATA_FAR IBCC_FAR  0xF88000 TO 0xF8BFFF;

      PAGE_F9       = READ_ONLY   DATA_FAR IBCC_FAR  0xF98000 TO 0xF9BFFF;

      PAGE_FA       = READ_ONLY   DATA_FAR IBCC_FAR  0xFA8000 TO 0xFABFFF;

      PAGE_FB       = READ_ONLY   DATA_FAR IBCC_FAR  0xFB8000 TO 0xFBBFFF;

      PAGE_FC       = READ_ONLY   DATA_FAR IBCC_FAR  0xFC8000 TO 0xFCBFFF;

/*    PAGE_FD       = READ_ONLY                      0xFD8000 TO 0xFDBFFF; intentionally not defined: equivalent to ROM_4000 */

      PAGE_FE       = READ_ONLY   DATA_FAR IBCC_FAR  0xFE8000 TO 0xFEBFFF;

/*    PAGE_FF       = READ_ONLY   0xFF8000 TO 0xFFBFFF; intentionally not defined: equivalent to ROM_C000 */

END

PLACEMENT /* here all predefined and user segments are placed into the SEGMENTS defined above. */

      _PRESTART,              /* Used in HIWARE format: jump to _Startup at the code start */

      STARTUP,                /* startup data structures */

      ROM_VAR,                /* constant variables */

      STRINGS,                /* string literals */

      VIRTUAL_TABLE_SEGMENT,  /* C++ virtual table segment */

    //.ostext,                /* eventually OSEK code  */

      NON_BANKED,             /* runtime routines which must not be banked */

      COPY                    /* copy down information: how to initialize variables */

                              /* in case you want to use ROM_4000 here as well, make sure

                                 that all files (incl. library files) are compiled with the

                                 option: -OnB=b */

                        INTO  ROM_D000;

      DEFAULT_ROM       INTO           PAGE_FE,          PAGE_FC, PAGE_FB, PAGE_FA, PAGE_F9, PAGE_F8,

                              PAGE_F7, PAGE_F6, PAGE_F5, PAGE_F4, PAGE_F3, PAGE_F2, PAGE_F1, PAGE_F0,

                              PAGE_E7, PAGE_E6, PAGE_E5, PAGE_E4, PAGE_E3, PAGE_E2,

                              /* PAGE_E1 intentionally not listed: assigned to XGATE */

                              /* PAGE_E0 intentionally not listed: assigned to XGATE */

                              PAGE_E0_0;

      //XGATE_STRING_FLASH,     /* XGATE strings that should always go into flash */

      //XGATE_CONST_FLASH,      /* XGATE constants what should always go into flash */

      //XGATE_CODE_FLASH        /* XGATE code that should always run out of flash */

      //                  INTO  PAGE_E0, PAGE_E1; /* FLASH accessible by XGATE */

    //.stackstart,            /* eventually used for OSEK kernel awareness: Main-Stack Start */

//      SSTACK,                 /* allocate stack first to avoid overwriting variables on overflow */

    //.stackend,              /* eventually used for OSEK kernel awareness: Main-Stack End */

      DEFAULT_RAM             /* all variables, the default RAM location */

                        INTO  RAM;

      SHARED_DATA             /* variables that are shared between CPU12 and XGATE */

                        INTO  RAM;

      XGATE_VECTORS,          /* XGATE vector table has to be copied into RAM by HCS12X */

      XGATE_STRING,           /* XGATE string literals have to be copied into RAM by HCS12X */

      XGATE_CONST,            /* XGATE constants have to be copied into RAM by HCS12X */

      XGATE_CODE,             /* XGATE functions have to be copied into RAM by HCS12X */

      XGATE_STRING_RAM,       /* XGATE strings that should always go into RAM */

      XGATE_CONST_RAM,        /* XGATE constants what should always go into RAM */

      XGATE_CODE_RAM,         /* XGATE code that should always run out of RAM */

      XGATE_DATA              /* data that are accessed by XGATE only */

                        INTO  RAM_FA, RAM_FB, RAM_FC /*, RAM_FD */;

      SSTACK

                        INTO  RAM_FD;

      PAGED_RAM               /* there is no need for paged data accesses on this derivative */

                        INTO  RAM;

      XGATE_STK_L       INTO  RAM_XGATE_STK_L;

      XGATE_STK_H       INTO  RAM_XGATE_STK_H;

    //.vectors          INTO  OSVECTORS; /* OSEK vector table */

END

ENTRIES /* keep the following unreferenced variables */

    /* OSEK: always allocate the vector table and all dependent objects */

  //_vectab OsBuildNumber _OsOrtiStackStart _OsOrtiStart

END

STACKSIZE 0xBB8   /* size of the stack (will be allocated in DEFAULT_RAM) */

/* use these definitions in plane of the vector table ('vectors') above */

VECTOR 0 _Startup /* reset vector: this is the default entry point for a C/C++ application. */

//VECTOR 0 Entry  /* reset vector: this is the default entry point for an Assembly application. */

//INIT Entry      /* for assembly applications: that this is as well the initialization entry point */


0 项奖励
回复
7,778 次查看
kef
Specialist I

      SSTACK

                        INTO  RAM_FD;

^^ this answers why

  • The value of the pointer should read: 00001B9C, which is not unpagined RAM (0x2000 TO   0x3FFF).
  • How is such thing possible? Thanks for your answer.

7,778 次查看
leroy_o
Contributor III

Thanks for your answer.

Yes. I assume there is no drawback to put the stack in pagined RAM, but I am a beginner on the S12X.

Maybe I am wrong, but in that case, shouldn't I read FD1B9C instead of 1B9C for the value of the pointer?

0 项奖励
回复
7,778 次查看
CompilerGuru
NXP Employee
NXP Employee

> Yes. I assume there is no drawback to put the stack in pagined RAM


Well one drawback is that a normal pointer cannot reliably point to a local variable anymore.

I would not locate the stack in paged RAM.

> shouldn't I read FD1B9C instead of 1B9C for the value of the pointer

Not sure why you are expecting that, a 16 bit pointer cannot contain a 24 bit address.

Not 100% sure, but I think locals are always expected to be non paged.

Daniel

7,778 次查看
leroy_o
Contributor III

Thanks for your answer.

Then it is also true for global variables because I did the test with moving the U8 buffer[8] variable from local to global and there is the same problem.

0 项奖励
回复
7,778 次查看
leroy_o
Contributor III

Addendum 2:

func1 is located at address: F987C9

func2 is located at address: F78B84

0 项奖励
回复