9S12D - General question

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

9S12D - General question

4,021 Views
prog_ram
Contributor III
Hi,
I have a simple question,
If we use the S12 D family MCU's, are there any differences between the D-family members in term of the configurations for their modules?
in other words, the code to configure the ATD (for example) module for the s12dp512 would be the same for any other D family member?
and how about configuring the osillator, is it the same for all D family?
thanks,

Message Edited by Alban on 2007-02-01 05:50 PM

Labels (1)
0 Kudos
Reply
4 Replies

2,093 Views
mke_et
Contributor IV
You're going to find the code is the same across just about the entire family is the same, but the 'configurations' will be different as appropriate for the actual chip you are using.

For example, I did all my development using what was called the 9S12Badge. This device had a 9S12DP256B part on it. When I wanted to develop for a project, I 'wire wrapped' in the badge for the project. Then, wheh the first batch of boards were made, using something like a 9S12A128 or whatever, I would just mount down the new chip and adjust my configuration to match.

Where things can get tricky concerns things like overlaps of EEPROM, registers, and SRAM. Or using I2C vs bit bang. Or page management of the flash, for example.

And some parts have other considerations. For example, a pin restricted part may need pins that are not bonded out to be treated a bit differently in software, to make sure they are benign, even though you didn't necessarily have to do that on parts that had the pins bonded out kind of thing.

Yes, there are always issues, but the parts of a family are all 'generally built from the same building blocks and that shouldn't be an issue.

Mike
0 Kudos
Reply

2,093 Views
prog_ram
Contributor III
thanks for the explanation..
0 Kudos
Reply

2,093 Views
Lundin
Senior Contributor IV
Apart from memory mapping issues you might also get problems if you are using an evaluation board with an old mask set (like the Future badge board does). The old "B" masks of DP256 didn't support Pierce ocillator while the old masks for DG128 did. This is pretty undocumented, but if you look in the older datasheets of Dx256, they actually don't mention the Pierce oscillator.

There are also loads of other silicon bugs in the old masks. My advice if you buy an old EBV is to replace the mcu with a new one, preferably of the derivate you plan to use in production.
0 Kudos
Reply

2,093 Views
Alban
Senior Contributor II
Hi,
My 0.02€, I 100% agree with Lundin.
We should always try and use the latest mask sets as they include fixes of old problems.
Also, it is the best way to predict the behaviour of the production application.
 
With the Sample Program, most parts are available COMPLETELY free of charge...
No cost to be up to date !
 
Cheers,
Alban.
0 Kudos
Reply